Mobile Synchronize

Exchanges incoming and outgoing packets between the local (enterprise) and remote (field) transporter directories regardless of whether the user is in the field or on the enterprise.

Enabled

  • A Database ID value must exist in the field database.

  • Checks that the MM_Mobile_State table exists.

Execute

  1. Locks out other transporter operations.

  2. Allows the transporter to synchronize with the enterprise.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.