Optional Feeder Manager 2.0 Configuration

Visit the topics below for further Feeder Manager 2.0 configuration options and details.

Feeder Manager 2.0 Field Visibility

When Feeder Manager 2.0 is enabled, certain fields are not visible in certain places.

Find Feeder Tool Stats Tab Troubleshooting

The data presented in the Stats tab of the Find Feeder tool depends on the proper configuration of your database. Explore this topic if your Find Feeder tool isn't displaying what you expect

Microsoft Esent and local storage

Microsoft Esent supports the local storage mechanism of Feeder Manager 2.0. There are a variety of registry key values that you can use to adjust the way Esent works with Feeder Manager 2.0.

Validation Rules

Feeder Manager 2.0 contains a variety of new validation rules you can assign to ensure the correctness of your data (such as QA/QC and Editing Features).

Feeder Manager 2.0 data on ArcFM Server

With a pair of Esri patches, ArcFM Server supports viewing (but not editing) Feeder Manager 2.0 data.

Field Order

Feeder Manager 2.0 field groups can be configured to show at the top of your attribute table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.