Send Session to Enterprise

Takes a session from the mobile environment and puts it back on the enterprise server.

Enabled

  • The MM_Mobile_State table must exist in the current Process Framework database.

  • The Database ID field must have a value. This field is located in the Process Framework Administration Tool on the Extensions tab.

  • MMSessionManager must be the current extension.

  • The selected node must be a session.

Execute

  1. Closes the session if it is open in ArcMap.

  2. Adds the packet to the transporter.

  3. Deletes the session.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.