Change Owner to Self

Changes the owner of the selected node to the current user.

Enabled

  • The node passed to this subtask must be a design or work request.

  • If the node passed to the subtask is a work request, the user must be on the enterprise. Users cannot change the owner of a work request in the field.

  • At least one user must exist in the MM_PX_USER table.

Execute

Changes the owner of the node to the current user.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.