Dearchive Packets

Decompresses the mobile packet using the selected encoder. If the dearchive subtask fails, all other subtasks will not run and prior subtasks will be rolled back.

Enabled

  • The node passed to this subtask must not be locked.

Execute

  • Decompresses the packets associated with the current node and its children using the transporter's "encoder." If a node is locked, it will not be decompressed and dearchived. A message will be sent to the event log and the subtask will continue to the next node.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.