Update License File

Use the License Updater to install ArcFM Solution licenses. The License Updater is located on the license server.

  1. From the Start menu, select ArcFM Solution | License Manager | License Updater.
  2. Click the Browse button and locate the license file (.xml) you received from Schneider Electric. The products and numbers of licenses for each are displayed in the Summary window.
  3. Click Install. The license files are installed.
  4. Click Exit to dismiss the License Updater utility.

    To request additional licenses, contact Schneider Electric.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.