Is Enterprise Disk Full?

Checks for free space based on a threshold value set in the MM_PX_CONFIG table. This threshold is set using the Configuration tab in the Process Framework Administration tool.

Enabled

  • Always enabled.

Execute

  1. Checks for free space on the disk on which the Enterprise base directory resides.

  2. Subtask fails if insufficient disk space exists.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.