Create CircuitSourceID Table

Feeder Manager 2.0 uses the CircuitSourceID table to store Subsource and UltimateSource information for your multi-tiered network.

Before creating the CircuitSourceID table, determine whether you want to use Object IDs or Global IDs.

Object IDs: Use the ObjectID field, which you can create manually. ObjectID has the data type Object ID.

Global IDs: Alternatively, you can use Global IDs. If you have a good reason to globalize your network features, e.g., you are running replication, then follow this approach. The GlobalID field has a data type of Global ID and may not be created manually. To create this field, right-click the CircuitSourceID table after it has been created and select Add Global IDs. This creates the field.

Choose only one of the options listed above.

CircuitSourceID

Field

Data Type

Domain

GlobalID

This field is created when you run the Add Global IDs tool in ArcCatalog. It cannot be created manually. Right-click the CircuitSourceID table and select Add Global IDs.

Global ID

Reset After Create = Yes
Visible = Yes
Editable = No

FeederLevel

Long integer

 

FeederName

Each value in this field must be unique. This field should have a NOT NULL constraint applied as well. Further, we strongly recommend that you set a unique constraint on this field.

text (length=48)

 

ObjectID

Object ID

 

SubstationID

Text

No domain
This field is required ONLY for Responder and Network Adapter/DMS implementations.

This field is not maintained automatically.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.