Create Session

Adds a new session node.

Enabled

  • MMSessionManager must be the current extension.

  • The selected node must be a filter (top level) node.

Execute

  1. Creates a new session node.

  2. Assigns the TypeID if one has been specified in the parameter.

  3. Adds the node to the TOC.

Parameters

  • SessionTypeID: Takes a session type (e.g., Electric, Gas, Water).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.