Create Packet

Creates a new mobile packet.

Enabled

  • A session or design node must be selected.

Execute

  1. Gets packet IDs and a file path.

  2. Creates a unique GUID for the packet.

  3. Creates a mobile packet for the selected node, saves its contents and closes it.

Parameters

  • OverrideDefaultPacketPrefix: takes a string value for the packet prefix that will override the default. If the parameter is not set, the defaults are used. The defaults are "MMSM_" for Session Manager and "MMWMS_" for Workflow Manager.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.