Welcome and FAQs

Welcome to the Desktop Configuration Guide.

Here are some tips to help you find relevant information fast:

  • Topics are organized thematically in the Table of Contents along the left-hand side. Expand topics to reveal subtopics.

  • Use the Search field to type keywords you’re looking for. The Search defaults to querying within the current guide, but it also gives you the chance to query the entire catalog of guides. Further, it allows you to filter by product, guide type, and version. Enter your search terms to get started.

    Watch this short video that walks you through how to perform a search and filter your results.

  • While reading a topic, press the down key to scroll down through the topic, press the right key to move to the next topic in the Table of Contents, and press the left key to move to the previous topic in the Table of Contents.

  • Want to send a topic to a co-worker? Click the Sharable Link tool. This copies the current topic’s URL straight to your clipboard, ready for you to paste into an email or other message.

    Want to see how the Shareable Link tool works in action? Watch this short video!

  • Is the image a little too small? Click it to open in a separate tab. It opens as large as possible.

  • Use the “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively. The following video explains how the “Was this helpful?” button works.

  • Watch this video to learn more about navigating the ArcFM Solution Documentation Portal.


Frequently Asked Questions (FAQ)

What’s the user community searching for? Here are the top searches and topics visited in this guide:

Desktop Config
  1. What is the difference between Feeder Manager 1.0 and Feeder Manager 2.0?

    1. Feeder Manager 1.0 is the original version of Feeder Manager. It tracks and updates feeder information by using your geodatabase. This version incurs substantial database querying and updates. Compared to Feeder Manager 2.0, you'll experience reduced performance and greater likelihood of version conflicts. However, third party customizations might be easier to implement since the feeder information is stored in a readily accessible geodatabase field. Feeder Manager 2.0 tracks feeder information in memory. Performance is far superior to that of Feeder Manager 1.0, and you can expect fewer version conflicts. Accessing feeder information outside of ArcMap, however, requires running the Feeder Export or other geoprocessing tools, and it may require you to update existing customizations.

      Schneider Electric strongly recommends Feeder Manager 2.0, but you can read all the details in the Feeder Manager topics and make an informed decision.

  2. How many different ways can I configure the ArcFM Abandon tools?

    1. Your users have two tools available: ArcFM Abandon and ArcFM Abandon and Remove (and a third tool called Convert to Conduit for linear features that can be performed after the abandon). And, you have four possible configurations: Abandon to Object Class, Abandon to Feature Class, Abandon to Subtype, and Abandon to Indicator Field. So, don’t let the tool names confine you, because you can assign any one of the four functions to each of the abandon tools. In other words, pick the two functions you want, then assign them to the two tools. It is better to think of them as Abandon Method #1 and Abandon Method #2. Abandon to Object Class is typically coupled with ArcFM Abandon and Remove, but again, it does not have to be. If you want to have Method #1 be Abandon to Feature Class and Method #2 be Abandon to Indicator field, that is perfectly possible. You can even rename the tools to match their configured function!

      See the topic Configure Abandon Tool for all the possibilities.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.