Set to Standard Design

Changes the product type of the selected design node (e.g., express design or stake job) to be a design.

Enabled

  • A design or work request node must be selected.

  • MMWorkflowManager must be the current extension.

Execute

  1. Gets the design.

  2. Sets the mmWMSDesignerProductType enumeration value to mmDesigner.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.