Add Fields

Add the fields to the following feature classes. The ParentCircuitSourceID or ParentCircuitSourceGUID field (but not both) must be added to ALL features that participate in the electric geometric network. The CircuitSourceID (or CircuitSourceGlobalID and CircuitSourceGUID fields) and Subsource fields must be added to any feature classes that may be designated as subsources and/or ultimate sources. This page provides examples. You may wish to use different features as subsources and ultimate sources.

BusBar:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Conductors (primary and secondary):

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Delivery Point and Generator:

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

Misc Network Features:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Network Junctions:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Open Point:

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

PF Correcting Equipment:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Primary Meter:

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

Protective Devices (Dynamic Protective Device and Fuse):

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

Service Point:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Streetlight:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Switch:

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

Transformer:

Field

Data Type

Domain

CircuitSourceGlobalID

Global ID

No domain
Default value = null

CircuitSourceGUID

GUID

No domain
Default value = null

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

Subsource

short integer

Yes/No domain
Data type = 16-bit integer
Default value = null

Voltage Regulator:

Field

Data Type

Domain

ParentCircuitSourceGUID

GUID

No domain
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added the feature will not work with Feeder Manager.

ParentCircuitSourceID

long integer

No domain
Data type = 32-bit integer
Default value = null

FacilityID

text (length=20)

No domain
Default value = null

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.