Convert to XML Packet

Takes an existing workspace packet (older functionality) and converts it to an XML packet (new and more efficient functionality).

Enabled

  • A session or design node must be selected (Enterprise or field database).

Execute

  1. Checks to see that packet conversion applies. The node must be a session or design, it must be unlocked, and the user must have an MMSessionManager or MMWorkflowManager extension.

  2. Looks at the MM_MOBILE_STATE table to see if the session or design node has a corresponding row.

  3. Determines whether the node has a  workspace packet. If it doesn't, the subtask exits.

  4. Gets the path to the workspace packet.

  5. Converts the workspace packet to an XML packet.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.