Undo Approved Design

Changes the design’s status from Approved to Pending Approval.

Enabled

  • MMWorkflowManager must be the current extension.

  • The selected node is a design node.

Execute

  1. Removes the values for the Approved Date and Approved By ID properties in the design.

  2. Removes the corresponding entry in the MM_WMS_APPROVED_DESIGNS table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.