Close Design

Closes a design that has been opened in ArcMap

Enabled

  • MMWorkflowManager must be the current extension.

  • The node passed to this subtask is a design node.

  • Workflow Manager must be open through ArcMap.

  • A design must be open in ArcMap.

Execute

  1. Closes the open design.

  2. Sets the PxApplication on the Process Framework Tasks tool extension to nothing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.