Add Model Names to Domains

Ensure the following model names have been added to the Gas Object Class Model Name domain, the Gas Field Model Name domain, and the Domain-Independent Field Model Name domain. If they do not exist, you will need to add the model names to the appropriate domain.

Model Names

Field Model Names

Domain-Independent Field Model Names

CONTROLFITTING

BONDEDINDICATOR

AMPS

CPPIPE

CPSYSTEMSTATUS

DESCRIPTION

CPSYSTEM

EMERISOLATIONSYSSTATUS

INSERVICEDATE

DISTRIBUTIONMAIN

GASPRESSURESYSTEMSTATUS

VOLTS

GASNONTRACEABLE

GASSYSTEMSTATUS

 

GASNETWORKEDGE

GASTRACEWEIGHT

 

NONCONTROLFITTING

INSULATEDINDICATOR

 

RECTIFIER

MATERIAL

 

REGULATOR

MEASUREDLENGTH

 

SERVICE

NORMALPOSITION

 

SPLITTARGET

OPERATINGCLASSIFICATION

 

SQUEEZEOFF

OPERATINGPRESSURE

 

NETWORKSOURCE

PIPEDIAMETER

 

TESTPOINT

PIPESTATUSINDICATOR

 

VALVE

PIPETYPE

 
 

SOPIN

 
 

SOPOUT

 
 

STATUS

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.