GDBM Set Posting Priority

Assigns the posting priority set in Geodatabase Manager to the corresponding session or design version.

Enabled

  1. Process Framework must have been started from within ArcMap.

  2. The selected node must be a session or design.

Execute

  • Writes or updates a row in the GDBM_Post_Queue table for the node's version.

Parameters

  • Priority: Sets the post priority on the version. The default is 0, which is the lowest priority.

  • ShowMessages: Determines whether the application displays message boxes if problems occur while subtasks are executing. The default setting is True. If the user sets this value to False, the application does not display message boxes but errors and warnings are still recorded in the operating system's error log. For Windows, this file is accessed from the Computer Management console. Navigate to the Event Viewer > Applications and Services Logs > Miner node to view applicable messages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.