Restore Subtasks

By default, the transporter copies packets to a backup folder before it decodes the file to the working folder. After the transporter decodes the packet to the working folder, Process Framework will attempt to read the packet into the PX tables. If successful, then the backed up, compressed packet will be deleted.

So, if a user executes Send/Receive and one of the packets fails to update the PX tables, the "Restore" subtasks below are a way to restore the backup of the compressed packets back to the incoming folder.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.