Service Point

Object Model names: FdrMgrLoadPoint

Note for Responder Users: The FdrMgrLoadPoint model name may be assigned differently depending on your data model. Refer to the Responder documentation for information about assigning this model name. It is strongly recommended that you assign this model name during the initial Feeder Manager configuration to avoid the need to re-initialize trace weights during Responder configuration.

Note for All Other Users: The FdrMgrLoadPoint model name is required for load point counting (counting affected customers) in ArcFM Mobile. It is strongly recommended that you assign it during the initial Feeder Manager configuration to avoid the need to re-initialize trace weights at a later time.

Field Model names:

Field

Field Model Name

Properties

FeederID

FeederID

Field Info Tab:

Reset After Create = Yes

FeederID2

FeederID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FeederInfo

Field Info Tab:

Editable = No

Reset After Create = Yes

ElectricTraceWeight

MMElectricTraceWeight

Field Info Tab:

Reset After Create = Yes 

PhaseDesignation

PhaseDesignation

 

ServiceCurrentRating

ServiceCurrentRating

 

Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network.

ParentCircuitSourceGUID

ParentCircuitSourceGUID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

ParentCircuitSourceID

Field Info Tab:

Visible = Yes

Editable = No

Reset After Create = Yes

FacilityID

FacilityID

Field Info Tab:

Visible = Yes

Editable = Yes

Reset After Create = No

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.