Configure Availability Indicator

To configure the Availability option for use in your geodatabase, follow these steps:

  1. Add the following field model name to the Electric Field Model Name domain.

    DUCTAVAILABILITY

  2. Create the Duct Availability domain with a data type of Text. The Duct Availability domain is used to indicate whether a conduit can accept additional conductor. The default should be set to 1 to indicate the duct is available.

    Availability

    Coded Value

    Unavailable

    0

    Available

    1

  3. Add the following fields to the DuctDefinition object class.

    Field Name

    Data Type

    Domain

    Available

    text

    Availability Indicator

  4. Assign the following field model name to the DuctDefinition object class.

    Field

    Field Model Name

    Available

    DUCTAVAILABILITY

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.