Configure ArcFM Phase Swap

The Phase Swap tool allows users to switch a branch of existing energized feeder from one phase to another. The following model name and field model names must be assigned. In addition, this tool also requires configuration of Feeder Manager (see below).

Model Name

Feature Class

Model Name

TransformerUnit

TRANSFORMERUNIT

Field Model Names

Feature Class

Field

Field Model Name

Transformer

RatedkVA

RATEDKVA

TransformerUnit

RatedkVA

RATEDKVA

This tool requires configuration of Feeder Manager, which includes the following field model names:

Feature Class

Field

Field Model Name

Domain

Any feature class that may participate in Phase Swap

Phase Designation

PHASEDESIGNATION

On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase.

Any switchable device that may participate in Phase Swap

NormalPosition_A

NORMALPOSITION_A

Normal Status

Any switchable device that may participate in Phase Swap

NormalPosition_B

NORMALPOSITION_B

Normal Status

Any switchable device that may participate in Phase Swap

NormalPosition_C

NORMALPOSITION_C

Normal Status

Omit Features from Phase Swap

Assign the DISABLEPHASESWAP model name to any feature class that you wish to omit from Phase Swap. The Phase Swap tool will ignore any feature class with this model name assigned.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.