Switch to Parent Version

Changes the version to the current version’s parent. Users might choose to use this subtask after closing, deleting, or posting a session.

Enabled

  • This subtask is always enabled.

Execute

  1. Ensures there is no editing session started. If one is started, warns the user to end the editing session.

  2. Opens the current version’s parent.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.