Busbar

Event

Autoupdater

On Feature Create

ArcFM Create Feeder Object

On Feature Update

ArcFM Update Feeder Object

On Feature Delete

ArcFM Delete Feeder Object

Before Feature Split

none

On Feature Split

ArcFM Split Feeder Object

After Feature Split

none

Optional: The following autoupdaters are required only if you have a multi-tiered network, and they should be assigned to all edge features in the electric network.

On Feature Create

Remove the ArcFM Create Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Level

  3. ArcFM Internal FeederID Create

 

On Feature Update

Remove the ArcFM Update Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Level

  3. ArcFM Internal FeederID Update

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.