Change Owner All Session

Changes the owner of a session to any valid user.

Enabled

  • MMSessionManager must be the current extension.

  • The node passed to this subtask must be a session.

  • Determines if there are any other users that have a role that can access the node in its current state.

Execute

  1. Identifies the users with the appropriate roles assigned to own the selected node.

  2. Gets the value of the DefaultUser parameter.

  3. If the AutoChangeOwner value is set to 1 (True), selects the DefaultUser and assigns the node. If no DefaultUser value is set, allows the user to select from a list of valid users.

  4. If the AutoChangeOwner value is set to 0 (False), selects the DefaultUser and allows the user to change the selection from a list of valid users. If no DefaultUser value is set, allows the user to select from a list of valid users.

  5. Assigns the node to the chosen user.

Parameters

  • DefaultUser: takes a user name as a value. The default value is null.

  • AutoChangeOwner: takes a value of 0 or 1. 0=False, prompt the user to select owner; 1=True, select default owner without prompt. The default value is 0 (False).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.