Configure Display Name Object

Custom display name objects allow you to include multiple attributes in the display name. If you have created a custom display name object, it can be assigned to features or related objects on the Field Display tab of the ArcFM Solution Properties Manager. Select a custom display name object from the Display Name Object field. Any value selected in this field overwrites what is selected in the primary display field.

IMPORTANT: Designer Users: Compatible Units (CUs) in Designer may not use Display Name objects. However, the Design, Work Location, and Work Request feature classes may use display name objects. If a display name object is assigned to one of these fields, it isn’t visible until the design is saved.

Sample Display Name Objects

Sample display name objects are available on the following feature/object classes with the ArcFM installation: CPSystem, DistributionMain, GasValve, Transformer, TransformerUnit. These samples require the following model names be assigned:

CPSystem Display Name Object

Model Name: CPSYSTEM

Field Model Names:

Field

Field Model Name

ID

ID

ProtectionType

PROTECTIONTYPE

Distribution Main Display Name Object

Model Name: DISTRIBUTIONMAIN

Field Model Names:

Field

Field Model Name

OperatingPressure

OPERATINGPRESSURE

NominalDiameter

PIPEDIAMETER

Material

MATERIAL

Valve Display Name Object (Gas and Water)

Model Name: VALVE

Field Model Names:

Field

Field Model Name

FacilityID

FACILITYID

ValveSize

VALVESIZE

Material

MATERIAL

Transformer Display Name Object

Model Name: TRANSFORMER

Field Model Names:

Field

Field Model Name

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

RatedKVA

RATEDKVA

Transformer Unit Display Name Object

Model Name: TRANSFORMERUNIT

Field Model Names:

Field

Field Model Name

FacilityID

FACILITYID

PhaseDesignation

PHASEDESIGNATION

RatedKVA

RATEDKVA

Assign Display Name Objects

Once you have created a custom display name object or configured the samples provided with the ArcFM install, the display name objects must be assigned.

  1. Select a feature or object class in the Catalog Tree.
  2. Click the ArcFM Properties Manager button on the ArcFM Solution toolbar OR right-click a feature class and select ArcFM Properties Manager.
  3. Select the Field Display tab.
  4. When a custom display name object is registered in the correct category, it will appear in the Display Name Object field. Select a value from the Display Name Object pulldown menu. The example depicts selecting Valve Display Namer from the Display Name Object pulldown. This value overwrites what is selected in the Primary Display Field.
  5. You must select a value for the Primary Display Field as well. This value is always used by the ArcFM Display Field locator.
  6. Click Apply to save edits and retain the Properties Manager OR click OK to save edits and dismiss the Properties Manager.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.