Processors

Use this tab to assign message processors to handle messages to/from an external application (e.g., WMS).

Field Descriptions

Type

Identifies the format of the incoming message (e.g., CIM).

Verb

The action to be performed (e.g., updated, created, deleted, get, executed, show).

Noun

The object on which the action is performed (e.g., session, compatible unit, design, work request).

Version

The version associated with the incoming message.

Processor

Select your custom processor. This field is populated with objects in the M&M Process Framework Message Processors category. If your custom processor does not appear in this list, check to be sure it has been properly registered in the correct category.

Workflow Manager Sample Processors

These processors are provided with the WorkflowManager.mdb. All sample message processors below are for CIM-compliant messaging and require a Type value of CIM. Additional message processors may be added

Create Design

Indicates that a design has been created; the Workflow Manager database updates accordingly. This processor requires a Create verb and a Design noun.

Create Work Request

Indicates that a work request has been created; the Workflow Manager database updates accordingly. This processor requires a Create verb and a Work Request noun.

Delete Design

Indicates that a design has been deleted; the Workflow Manager database updates accordingly. This processor requires a Delete verb and a Design noun.

Delete Work Request

Indicates that a work request has been deleted; the Workflow Manager database updates accordingly. This processor requires a Delete verb and a Work Request noun.

Get Design

Retrieves a design. This processor requires a Get verb and a Design noun.

Get Work Request

Retrieves a work request. This processor requires a Get verb and a Work Request noun.

Update Design

Indicates that a design has been modified; the Workflow Manager database updates accordingly. This processor requires an Update verb and a Design noun.

Update Work Request

Indicates that a work request has been modified; the Workflow Manager database updates accordingly. This processor requires an Update verb and a Work Request noun.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.