Does User Own Session Node?

Checks to see if the user is also the current owner.

Enabled

  • If the user is not the owner, the Enabled method will return false and the subtask will be disabled.

Execute

  • Always returns true.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.