Duct Annotation Display Namer

The Duct Annotation Display Namer uses the annotation expression for a duct's members in the Attribute Editor, Diagram Manager, and Conduit Configuration dialogs.

This display namer is applied to feature classes (e.g. conductors and fiber cables) using the ULSMEMBER class model name.

The ULSMEMBER class must be related to an Annotation Class (e.g. PriUGAnno) which has the ULSMEMBERANNO class model name applied.

Once configured, the ULSMEMBERANNO class's rendering as seen in the map displays in the Attribute Editor, Diagram Manager, and Conduit Configuration dialogs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.