Mobile Update

Uses the current user's user name to update the field database with mobile packets from the Enterprise.

Enabled

  • The MM_Mobile_State table must exist.

  • The current Process Framework database must be a field database.

Execute

  1. Removes all packets from the transporter repositories.

  2. Places packets in the current user's working directory.

  3. Update the Process Framework, Session Manager, and Workflow Manager tables based on the packet contents.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.