Open Express Design for As-Built Editing

Opens the selected design for as-built editing in Designer Express.

Enabled

  • An express design node must be selected.

  • MMWorkflowManager must be the current extension.

  • Workflow Manager must be opened from Designer and visible.

Execute

  1. Gets the express design.

  2. Determines whether the express design should be opened as View Only.

  3. Creates the workspace for the express design.

  4. Opens the express design and disables the Design Palette tab.

  5. Updates the MM_PX_Versions table to indicate the design exists.

  6. Disables the Stored Items tool.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.