Re-Send Session to Field

Executes the "Send Session to Current Field Owner" task if the node’s current owner has the Session ALWAYS Mobile User role assigned.

Enabled

  • MMSessionManager must be the current extension.

  • The selected node is a session.

Execute

  1. Gets the node's owner.

  2. Executes the "Send Session to Current Field Owner" task if the node's owner has the Session ALWAYS Mobile User role assigned.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.