Transformers

Object Model names: TRANSFORMER

Field Model names:

Field

Field Model Name

Properties

FeederID

FEEDERID

Field Info Tab:

Reset After Create = Yes

FeederID2

FEEDERID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FEEDERINFO

Field Info Tab:

Editable = No Reset After Create = Yes

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

Field Info Tab:

Reset After Create = Yes

PhaseDesignation

PHASEDESIGNATION

 

Optional: Assign the following field model name if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage value. If this value doesn't exist (and the functionality is configured), the downstream secondary conductors inherit the OperatingVoltage value from the transformer.

LowSideVoltage

LOWSIDEVOLTAGE

 

Optional: Assign the following field model name if you want to display the Total RatedkVA for an electric trace. This functionality also requires model names on the TransformerUnit object.

RatedkVA

RATEDKVA

 

Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary sources.

ParentCircuitSourceGUID

PARENTCIRCUITSOURCEGUID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = Yes

CircuitSourceGlobalID

Global ID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = Yes

CircuitSourceGUID

GUID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = Yes

Add either only CircuitSourceID or both CircuitSoureGlobalID and CircuitSourceGUID, but not all three. If all three are added, the feature will not work with the manager.

CircuitSourceID

CIRCUITSOURCEID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = Yes

Subsource

SUBSOURCE

Field Info Tab:

Visible = Yes Editable = Yes Reset After Create = Yes

FacilityID

FACILITYID

Field Info Tab:

Visible = Yes Editable = No Reset After Create = No

NOTE: You may tap one or more of the available phases of a primary to provide service voltage. Feeder Manager uses the phase assignment of the transformer and voltage level attributes on conductor features to control tracing through the transformer. This allows Feeder Manager to correctly determine the status of the secondary and service wire when a single phase transformer taps a three phase line.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.