Open Point

Event

Autoupdater

On Feature Create

ArcFM Create Feeder Object

On Feature Update

ArcFM Update Feeder Object

On Feature Delete

ArcFM Delete Feeder Object

Optional: The following autoupdaters are required only if you have a multi-tiered network and you want to use open points as subsources.

On Feature Create

Remove the ArcFM Create Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Relator

  3. ArcFM Feeder Subsource Name

  4. ArcFM Feeder Subsource Level

  5. ArcFM Internal FeederID Create

 

On Feature Update

Remove the ArcFM Update Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Relator

  3. ArcFM Feeder Subsource Name

  4. ArcFM Feeder Subsource Level

  5. ArcFM Internal FeederID Update

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.