Send to Express

Takes a design from the mobile environment and puts it back on the enterprise server.

Enabled

  • The MM_Mobile_State table must exist in the current Process Framework database.

  • MMWorkflowManager must be the current extension.

  • The selected node must be a design.

Execute

  1. Gets the parent node of the selected design.

  2. Closes the design if it is open in ArcMap.

  3. Adds the packet to the transporter.

  4. Deletes the design and work request if it doesn't contain another design.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.