Approve Imported Design

Approves a design on the enterprise after it has been approved in the field and imported into the enterprise database.

Enabled

  • MMWorkflowManager must be the current extension.

  • The node passed to this subtask must be a design.

Execute

  1. Checks to see if the design has been approved and skips the design if it has not been approved.

  2. If any design in the same work request has already been approved, it will be unapproved.

  3. Approves the imported design on the enterprise.

  4. Checks the MM_PX_CONFIG table to see if the ConstructOnApprove flag has been set. If it is set, the Work Request is assigned the state of In Construction.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.