Restore Backup Packet

Pulls a specific packet from the transporter's backup folder and restores it to the working directory.

Enabled

  • The database must support Mobile.

  • A packet that corresponds to the selected packet ID must exist in the transporter's backup folder.

Execute

  • Pulls the packet from the backup folder and places it in the working directory.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.