Conductor (primary and secondary)

Event

Autoupdater

On Feature Create

ArcFM Create Feeder Object

On Feature Update

ArcFM Update Feeder Object or ArcFM Update UG Feeder Object

On Feature Delete

ArcFM OH (or UG) - Delete Feeder Conductor/Units

Before Feature Split

ArcFM Save Related Objects (Optional. This AU is available only if a relationship exists)

On Feature Split

ArcFM Split Feeder Object

After Feature Split

ArcFM Restore Related Objects (Optional. This AU is available only if a relationship exists)

Assign the following autoupdater to secondary conductor classes if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage value. If the LowSideVoltage value doesn't exist (and the functionality is configured) or the AU is assigned to the primary conductor, then the downstream secondary conductors inherit the OperatingVoltage value from the transformer. This autoupdater fires on the On Feature Update event only when the shape of the line is modified.

On Feature Create

ArcFM Inherit Operating Voltage

Optional: The following autoupdaters are required only if you have a multi-tiered network.

On Feature Create

Remove the ArcFM Create Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Level

  3. ArcFM Internal FeederID Create

 

On Feature Update

Remove the ArcFM Update Feeder Object AU and assign these:

  1. ArcFM Generic Electric Trace Weight

  2. ArcFM Feeder Subsource Level

  3. ArcFM Internal FeederID Update

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.