Set Snapping on DFCs

In order to place DFCs in the map, you will need to set the snapping properties on them. Use the ArcFM Snapping Manager in ArcCatalog. If you do not set the snapping properties, the features converted from DFCs may not be properly connected to the geometric network. Set DFCs to snap to other DFCs as well as existing feature classes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.