Network Junctions

Configure this class if you want your default junction features to carry an automatically updated FeederID. If you haven't yet created your geometric network, this feature class won't be available. You will need to configure it after creating the geometric network. This will be discussed later.

Object Model names: None

Field Model names:

Field

Field Model Name

Properties

FeederID

FEEDERID

Field Info Tab:

Reset After Create = Yes

FeederID2

FEEDERID2

Field Info Tab:

Reset After Create = Yes

FeederInfo

FEEDERINFO

Field Info Tab:

Editable =No
Reset After Create = Yes

ElectricTraceWeight

MMELECTRICTRACEWEIGHT

Field Info Tab:

Reset After Create = Yes

Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network.

ParentCircuitSourceGUID

PARENTCIRCUITSOURCEGUID

Field Info Tab:

Visible = Yes
Editable = No
Reset After Create = Yes

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceID

PARENTCIRCUITSOURCEID

Field Info Tab:

Visible = Yes
Editable = No
Reset After Create = Yes

FacilityID

FACILITYID

Field Info Tab:

Visible = Yes
Editable = Yes
Reset After Create = No

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.