Extensions

The Extensions tab allows you to list the extensions that are supported by the database to which you are currently logged in. Use the Add and Delete buttons to modify the list.

Database ID

The Database ID is a unique value that identifies the enterprise server. This allows multiple servers to use the same network to store mobile packets. An administrator must assign a unique value to each server. A valid value is required in this field only if you are using ArcFM Mobile or Designer Mobile. The Process Framework Administration Tool will not close until a value is entered in this field. If you are NOT configuring Mobile, enter any value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.