Has No WS Packet

Determines whether a design or session is associated with a workspace packet. This subtask can be used to disable tasks you do not want performed on designs or sessions associated with workspace packets by setting the parameter to true. If the parameter is set to true and a workspace packet is detected, this subtask will be disabled and cause the task to fail.

Enabled

  • If the parameter is set to false, this subtask is always enabled.

  • If the parameter is set to true, the open session or design must not have an associated workspace packet.

Execute

  1. If the parameter is set to false, the subtask always stays enabled. If the parameter is set to true, the subtask checks if the design or session is associated with a workspace packet.

  2. If the parameter is set to true and the design or session is associated with a workspace packet, the subtask is disabled.

  3. If the subtask is disabled, the task fails and an error message is displayed.

Parameters

  • ValidateOnEnable: Can be set to true or false. The default is false.

    • If set to true, the subtask checks if the session or design is associated with a workspace packet. If the session or design is associated with a workspace packet, the subtask is disabled.

    • If set to false (default), the subtask will not check for workspace packets. Instead, the subtask will always be enabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.