Add Model Names to Domains

Ensure the following model names have been added to the Water Object Class Model Name domain and the Water Field Model Name domain. If they do not exist, you will need to add the model names to the appropriate domain.

Model Names

Field Model Names

Domain-Independent Field Model Names

CONTROLFITTING

BONDEDINDICATOR

AMPS

CPPIPE

CPSYSTEMSTATUS

DESCRIPTION

CPSYSTEM

EMERISOLATIONSYSSTATUS

INSERVICEDATE

DISTRIBUTIONMAIN

INSULATEDINDICATOR

VOLTS

NETWORKSOURCE

MATERIAL

 

NONCONTROLFITTING

MEASUREDLENGTH

 

PIPE

NORMALPOSITION

 

RECTIFIER

OPERATINGCLASSIFICATION

 

REGULATOR

OPERATINGPRESSURE

 

SERVICE

PIPEDIAMETER

 

SPLITTARGET

PIPESTATUSINDICATOR

 

SQUEEZEOFF

PIPETYPE

 

VALVE

SOPIN

 

WATERNETWORKEDGE

SOPOUT

 

WATERNONTRACEABLE

STATUS

 
 

SUBTYPECD

 
 

WATERPRESSURESYSTEMSTATUS

 
 

WATERSYSTEMSTATUS

 
 

WATERTRACEWEIGHT

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.