Access System Level Licensing

If you're running License Manager on a machine with a Windows 7 operating system, you may have trouble accessing the options necessary to control system-level licensing in the Desktop Administrator. In this case, the System field on the Software Product tab is disabled. On the License Manager tab, the "Show license expiration warnings to all users" checkbox is disabled.

To open Desktop Administrator with these fields enabled, right-click Desktop Administrator on the Start menu (Start > All Programs > ArcFM Solution > License Manager 9 > Desktop Administrator) and select Run as Administrator.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.