Feature and Object Classes

Three important feature classes must exist in your geodatabase for the minimum Conduit Manager configuration. If they don't exist, you need to create them.

You can name your feature classes and fields anything that makes sense for your business. However, model names, which are assigned in a later step, must have the exact spelling and capitalization as provided.

IMPORTANT: A geometric network (e.g., UndergroundNetwork) must include only the feature classes that represent parts of the underground structure of a conduit system. Conductors or other cables such as fiber optics should NOT be members of the underground structure network, but should be included in their own networks, such as an electric network, or a communications network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.