Duplicate Feature Validation Rule

This object validation rule ensures that duplicate features are not created when you commission design feature classes in Designer Express. You would use this rule when running QA/QC after you commission design feature classes. For example, a support structure and a transformer that have the same geometry would be validated, however two support structures that have the same geometry would not be validated.  In the example, each support structure would generate a QA/QC error. This rule works only on features, not tables.

To enable:

  1. Open ArcCatalog to browse the database of interest.
  2. Right-click the feature that you want to have this rule.
  3. Select ArcFM Properties Manager from the right-click menu.
  4. Under the Object Info tab, select the checkbox labeled Duplicate Feature. Click OK. 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.