Open Design

Opens the design node in ArcMap.

Enabled

  • A design node must be selected and it must not have a verified state.

  • MMWorkflowManager must be the current extension.

  • Workflow Manager must be open from ArcMap and visible.

Execute

  1. Calls Terminate on Process Framework’s active control if the active control is an IMMPxControl2. This gives the form displayed in Process Framework a chance to cancel this operation or to take some action before it is unloaded.

  2. Opens the design.

  3. Sets the PxApplication on the Process Framework Tasks Tool extension.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.