Using the Feeder Sync Tool When Posting (Default Configuration)

  1. In ArcCatalog, right-click your Electric Geometric Network and select Configure Feeder Manager.
  2. From the Feeder Manager configuration window:
    • Clear the Feeder Manager 1.0 option (if enabled).

    • Select the Feeder Manager 2.0 option.

    • Expand the Advanced Configuration options. Select the Feeder Manager 1.0/Feeder Manager 2.0 Field Sync option.

    • Optionally set the Enable autoupdaters during field sync option to allow autoupdaters to fire during field synchronization.

    • Set the Target version for sync (SDE.DEFAULT by default).

  3. Click OK.
  4. Create or open a session or design in ArcMap.
  5. Perform typical editing operations (create/delete features, editing existing features, etc.) in that session or design.
    • Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).

    • Notice that the feeder information in the legacy fields (FeederID, FeederID2, and FeederInfo) do not update after each edit.

  6. Save the session or design. This will populate the MM_EDITED_FEATURES table.
    • You can add the MM_Edited_Features table to inspect its contents if necessary.

  7. Post the session or design to SDE.DEFAULT. The former Feeder Manager 1.0 fields now populate with the new feeder information (FeederID, FeederID2, and FeederInfo).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.