Is Design Locked?

Checks the design to determine if the opened design is locked.

Enabled

  • Disabled if the design’s node is locked and the design is not currently opened.

  • Disabled if the design is state locked.

  • Disabled if the design is non-postable.

  • MMWorkflowManager must be the current extension.

  • The selected node is a design node.

Execute

  • Always returns true.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.