Display Edit Log Report

Opens a report that displays all edits made to the currently open session or design.

Enabled

  • The open session or design must have an associated XML packet. This means the Create Packet subtask must also be assigned to the same node. You can assign it on either the Create Design/Session task or the Open Design/Session task.

Execute

  1. Reads the XML packet.

  2. Converts XML packet contents for display in HTML window.

  3. Uses a style sheet to convert the XML packet edit log to HTML for display in a web browser.

    IMPORTANT: The style sheet location is determined by the following registry key: HKEY_LOCAL_MACHINE\Software\Miner and Miner\Process Framework\Style Sheets\EditHistoryXSLPath\

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.